Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
EEPROM-Slide10

Pull-up resistors can also be added to the clock and data lines to optimize the I²C EEPROM design. Depending on the speed of the bus, a 2 or 10 resistor is used. To further optimize the system with minimized power consumption or maximized speed, Application Note AN1028 goes through the calculations to select the optimal resistor size.

PTM פורסם ב: