Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
EEPROM-Slide3

Another advantage is the wide density range of the I²C protocol, ranging from 128 bits to 1 Mbit. An I²C device also features a smaller die size for a specific density which allows for a lower cost per density and smaller physical dimensions. Many I²C devices have a WP pin that prevents writes to the array when activated which can be used to prevent unwanted writes during power up and power down. Finally, many I²C EEPROMs include address pins as an easy way to have multiple EEPROMs on a single bus while still only using two connections to the microcontroller (MCU).

PTM פורסם ב: