Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
PIC24F-Slide5

The second of the four variants is the KL2 variant, which is highlighted in blue on this slide. When compared to the KL1 variant, these devices feature twice the amount of Flash memory, to 8kB, and integrate a 10-bit A/D converter. Similar to the KL1 variant these devices are also available in 14- and 20-pin count packages.

PTM פורסם ב: