Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
iPass Slide 5
The iPass host connector is derived from the high-volume 0.8mm card-edge connector family that has been used across the industry, including SFP, XFP, and XPAK. The lower row of contacts has been redesigned to match the data rate capability of the upper row. iPass offers manufacturing advantages over other high-speed I/O in that it is an SMT connector which is assembled during standard component placement, using T&R packaging. Additionally, unlike other I/Os, it has no balance or center-of-gravity issues, also benefiting the manufacturing process. iPass was designed for RoHS compliance from the outset. As the saying goes, the bottom line is that iPass is a small, single-row SMT card-edge connector that offers users low applied cost.
PTM פורסם ב: