Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
RF Switch Connectors Slide 11

The MM126037 is also designed to be used in a high speed production environment, but has a built-in self alignment feature.  The probe can tolerate a total horizontal movement of +/- 0.7 mm while anchored in a test jig with an appropriately sized access hole (13.5 mm diam.).  In this case, the probe aligns itself to the receptacle while the receptacle remains in a fixed position.  Selection of either type of production test probe (fixed or floating) will depend on the customer’s particular test setup.

PTM פורסם ב: