Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
LED-Slide2

LCD, or liquid crystal displays, have been on the market much longer than OLEDs. This presentation will breakdown Newhaven Display’s Character displays for LCDs and OLEDs. Character displays are only capable of displaying numbers, letters, and symbols similar to those found on a standard keyboard. Newhaven’s standard Character LCD modules are monochrome, passive matrix displays with built-in pre-programmed font tables. Newhaven Display’s LCD Character displays come in industry standard sizes from 1 x 8 characters to 4 x 40 characters. These displays can be used as compatible replacements for some of Newhaven Display’s VFD modules. Key features that stand out for the standard LCD Characters are their low power and high brightness backlights, available in 8 different color options. These displays offer industry standard interfacing, using either serial or parallel interfaces, and 4 built-in font tables.

PTM פורסם ב: