Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
More Aspects of Driving External Loads

The weak buffer is used to hold the signal in a steady state after the one-shots have deactivated. If additional drive current is required, external pull-up or pull-down resistors can be added. The value can be calculated via a simple voltage divider network as shown here.

PTM פורסם ב: