Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Up Translation

Looking at the NXS device used in up translation mode, meaning that the device is driving from a lower voltage domain on the A-side to a higher voltage domain on the B-side. Before translating a high-level signal, the pass transistor conducts the low voltage on the A-side through to the B-side. As the input signal rises, the pass transistor will switch off when the voltage exceeds the gate voltage minus the threshold voltage. When the input voltage rises to approximately VCC divided by two, the one-shot will activate to speed up the rising edge of the signal via the PMOS driver. When translating a low-level signal, both sides will start at a high level. The input signal will drive the A-side low. The pass transistor will begin to conduct when the gate-to-source voltage exceeds the threshold voltage. The output port will then follow the input port towards the low level.

PTM פורסם ב: