Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Configurable and Combination Logic Slide 4

The Configurable Logic products from Nexperia are separated into three different segments. The 1G57, 1G58, 1G97, and 1G98 represent four different base device functions which each offer a wide variety of nine, or more configurable logic functions. In addition, Nexperia offers the 1T57, 1T58, 1T97, and 1T98 which are based upon the 1G series devices, but incorporate level translation as well. Finally, Nexperia offers the 1G99 base device function in a slightly larger package option that allows for support of an Output Enable function. The 1G99 offers a rich set of available standard and complex logic functions which are derivatives of the standard NAND, NOR, AND, OR, buffer, and inverter functions. Shown here in the diagram at the bottom of this slide, one can see the available standard logic functions in Nexperia’s Configurable Logic product family. In addition, several more complex derivatives of these functions are also available. For a complete listing of all available functions, please consult the Nexperia product datasheet for the appropriate device.

PTM פורסם ב: