Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Product List
LPC29xx Microcontrollers Slide 13
The flash module consists of a built-in signature generator that can produce a 128-bit signature (MISR) from a selected range in Flash memory. A typical use would be to verify the flashed contents against a calculated signature (e.g. during programming) The flash controller generates interrupts at the end of key operations like burning and at the end of an erase cycle. Similar interrupts are generated from the EEPROM. The flash memory has a special index sector that is normally invisible from the address space. By setting a bit in the Flash control register the index sector becomes visible at the flash base address and replaces all regular sectors. By writing to specific locations in this sector the following features can be enabled: JTAG access protection, storage of customer information, and sector security. Care should be taken while writing to the index sector, as this cannot be erased. The flash endurance is specified at a minimum of 100K write cycles with a retention specified at 10yrs.
PTM פורסם ב: