Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Product List
LPC29xx Microcontrollers Slide 64
Because of the ARM core’s widespread acceptance into various microcontrollers, many third party vendors provide development tools, demonstration boards, software, and compilers. The OM11014 from NXP and Keil allows creation and testing of programs for the advanced LPC2919 controller. One serial interface, an analog input (via potentiometer), two CAN interfaces, one LIN transceiver, LCD, and eight LEDs make this board a great starting point for LPC2900 projects. Similar boards will also be available for the LPC2929 and LPC2939, but at this time, DigiKey only stocks the OM11014.
PTM פורסם ב: