Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
AMCCS-Slide16

The cable collet components shown here saves the cable from being pulled out from the connector and damaging the termination points. Cable collets are used in all straight and in-line receptacles. It is important to correctly identify outer cable diameter measurements to match it to the correct collet size. The sealing ring is required to achieve the IP68 rating and the EMI ring is for transmission of the shielding.

PTM פורסם ב: