Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
heatsink-slide4

For the first example, a maximum case temperature of 95°C will be used with an ambient temperature of  25ºC and a power dissipation of 100 watts. These values result in 0.75 degrees C per Watt thermal resistance. When this value is applied to the chart with natural convection, a heatsink of approximately 105 cubic inches would be required. Only 20 cubic inches would be needed when forced air is applied.

PTM פורסם ב: