Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
heatsink-slide7

In summary, to be able to determine the proper heatsink for an application, the heatsink thermal resistance required for the application needs to be calculated. To calculate thermal resistance, several parameters are required including the maximum case temperature, ambient air temperature, and power dissipation. Ohmite offers several heatsink series appropriate for applications requiring different wattages and mounting options.

PTM פורסם ב: