Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
high freq

Step three is to confirm the high frequency characteristics of the desired relay. Isolation expresses the signal leakage level between open contacts; the larger the number, the better the leakage level will be. Insertion loss is the signal loss level between closed contacts; the smaller the number, the better the loss level is. Return loss expresses the ratio of reflected signal which occurs between the signal input and the transmission circuit; the larger the number, the lower the loss is.

PTM פורסם ב: