Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Cooling Fan Motor Drivers Slide 18

The application will dictate what type of motor drive method is preferred. If silent drive is the most important, then a BTL drive method for a single-phase motor should be chosen. If it is a mix of quietness and power, then a BTL-PWM driver is a good choice. If power, price, and quietness are the mix, then perhaps a PWM switched solution would be best. The items shown on this slide will further narrow down the selection process. If the customer is still unsure, they can contact applications support.

PTM פורסם ב: