Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Cooling Fan Motor Drivers Slide 19

The LV8163QA shown on this slide is a BTL control method 5 V fan motor driver. It includes the hall sensor bias circuitry in addition to PWM speed control. If the fan is blocked, lock protection circuitry will stop current from going to the motor and allow auto restart after some time has passed. The BTL drive combined with the PWM pulse yields a silent drive with high efficiency.

PTM פורסם ב: