Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Summary PalmSens' Archived Publications Page PalmSens' Support Email Analog Devices' EngineerZone Q&A Support Community Page

In summary, the main topics addressed in this presentation are electrochemistry which controls and observes the electric current to understand chemistry, and the EmStat Pico which is especially useful for electroanalysis. The EmStat Pico is also used for advanced applications like Covid-19 detection in point-of-care settings, to measure corrosion, or to detect a specific element in food to determine its quality. Support is available via support@palmsens.com or the ADI support forum. The EmStat Pico potentiostat module is available with all or a limited set of electrochemical techniques. The first prototypes typically have the EmStat Pico with all supported electrochemical techniques. An EmStat Pico with a limited set of techniques is also available for next design phases. Many electrochemical applications are possible, and all that is needed is the EmStat Pico development board.

PTM פורסם ב: