Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
USB-Switch-Slide3

The USB switch is a bidirectional device that selects one of several input USB signals and forwards the selected input into a single line or vice versa. Pericom’s USB switch uses the NMOS gate technology with charge pump on the gate which enables it to increase the voltage at the gate to avoid output voltage clamp caused by the threshold. The advantages of the charge pump are: Wider Vcc range, Rail to rail output voltage without clamp, and Low Coff and Con.

PTM פורסם ב:
PTM Updated on: 2015-04-13