Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
keyswitch-slide6

A few points relevant to system structure to consider are, depending on the keyswitch used, the illumination is either already built-in or is installed next to the keyswitch if required, the plunger is either placed on the keyswitch or is already built-in, the typical tactile properties of RAFI short-travel keyswitches can be ensured by maintaining the specified distance from the overlay to the PCB with distance bushings, and embossing over the keyswitches is recommended for an overlay.

PTM פורסם ב: