Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
8-15 Watts DC/DC Converters Slide 1
Welcome to the new RECOM 8-15 Watts DC/DC Converters for Medical and Telecom Markets product training module. This module will identify new applications for DC/DC converters in the 8 to 15 W power range, beginning with a review of the existing DC/DC converter limitations and the improvements in the new RECOM families of DC/DC converters for 8 to 15 W. Also, there will be an overview of their use in those new markets or applications. Finally a list of the related RECOM DC/DC controllers available at DigiKey will be presented.
PTM פורסם ב: