Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
FSDR-Slide20

The standby current consumption when the EN pin is low is typically 0µA. On this slide, figure 6 shows the operating current with EN high over the input voltage range. Depending on the output load and input voltage, power conversion efficiency for these ICs can be as high as 90%.

PTM פורסם ב: