Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
CMOS-Slide10

Shown here is another application example. In this case, an OpAmp is used for monitoring current detection. To monitor the motor current, a current detection resistor is installed to convert the current into voltage. However, the voltage difference at both ends is very small. The OpAmp amplifies the weak converted signal to a high enough level so that it can be processed by the MCU.

PTM פורסם ב: