Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Image of Sanyo Denki Improving Motor Performance - StepOut

Step-out is when a stepping motor has position misalignment. This can be caused by sudden change of speeds or an overload. An overload is when more power is applied to the motor shaft than the rated holding torque of the motor. The graph here gives a simple demonstration of where the motor would be under a stable position when the load torque of a system does not exceed the maximum torque of the motor.

PTM פורסם ב: