Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Image of Sanyo Denki Improving Motor Performance - Improve Torque Continued 1

Another way to improve torque at higher speeds would be to use a driver that can output a larger source voltage. In the graph, one can see the differences when using a 24VDC drive, 36VDC drive, and a 100VAC drive. Of course, this may then lead to increasing the cost in the system since the customer might need to use a higher rated power supply and driver.

PTM פורסם ב: