Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
select fan
The next step is to then find a fan that can provide the calculated airflow. A safety margin is usually included on the airflow result, and ranges from 130% to 200%. The designer can then cross-reference this airflow result with the catalog sheet of a fan size that can physically fit, to identify the closest match. Most commonly, a fan with more airflow is selected, which results in unnecessarily high noise and power draw.
PTM פורסם ב: