Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
summary
In summary, fan specifications shown in catalogs, like noise and power, are for conditions with no load. There is always a load on a fan in actual use, so these specifications will change depending on how a fan is used. A system curve is used to find the operating point of a fan in a chassis. Finally, choosing the right fan with regards to the operating point will minimize both noise and power consumption.
PTM פורסם ב: