Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
CP2130-Slide12

Silicon Labs provides a comprehensive driver suite with support for all major operating systems, including Windows, Mac OS X, Linux, and WinCE. Some of the drivers are natively supported within the operating system and do not require a driver installation. Those are marked with an asterisk in the table above. The interface specification is also provided to allow for developers to create their own driver if needed.

PTM פורסם ב: