Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
External Convert
For single battery applications, other devices need to use a standalone DC/DC converter. It is not possible to switch off an external boost converter, otherwise the MCU can never wake-up from sleep. Therefore, there is a big advantage in sleep mode current when the DC/DC converter is integrated on-chip. If the application needs more current, it is still very efficient to use C8051F900 with an external DC/DC converter because the C8051F900 will allow it to be switched completely off.
PTM פורסם ב: