Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Si100x/1x ISM Transceiver Family Slide 20
There are several modes to use when receiving data. If the FIFO is used, then there must be a preamble and sync word added to the transmitted data. If the packet handler is enabled, the header bytes and the packet length fields are included in the packet and it is controlled by the registers of the peripheral while the CRC checks the integrity of the data. If packet handling is disabled then the header bytes, packet length and CRC become part of the data transfer and must be maintained by the CPU when writing the data to the FIFO.
PTM פורסם ב: