Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Low Noise General Purpose Amplifiers Slide 6

The received signal is usually very low in signal strength. The LNA is designed to amplify these signals while contributing as little noise as possible to drive the next stage. The equations on this slide show how the noise at the input of a radio can significantly impact the noise of the over-all system and the receive sensitivity of the system.

PTM פורסם ב: