Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Multiple Sensing Point Application
  • Multiple sensing points
  • Stem circuitry

 Slide 12 GIF

Many liquid level sensing applications call for multiple detection points. This is an ideal application for the liquid level reed sensor. In this case all the circuitry is mounted on a PCB that is mounted within the stem. Typically a resistor is used in parallel with each sensing point. In this case, as the various reed switches are energized the overall resistance changes. This information is input to a computer that converts this change in resistance to the latest level, which then sends this information to a read-out mechanism or to the end user.

PTM פורסם ב: