Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Liquid Level Sensing Technology Slide 2

There are three typical liquid level sensing approaches. One approach uses inductance to sense motion, the second uses a direct connection from a float that mechanically moves a contact switch, and the third approach uses a float with an embedded magnet that activates a reed switch. The inductive approach is expensive and requires a lot of circuitry. The mechanical approach can easily get clogged and is subject to failure in dirty environments. For these reasons this presentation will focus on the reed sensor technology, which is being implemented in many applications.

PTM פורסם ב: