Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Reed Relay Overview Slide 4

The pull-in voltage is that point where the contacts close while the voltage is slowly ramping up. Conversely, the dropout voltage is the point where the contacts open while slowly ramping down the voltage. The voltage measurement for pull-in and drop-out is made directly across the coil. The resistance of the copper wire making up the coil is called the coil resistance. Hysteresis is the ratio of the drop-out voltage to the pull-in voltage, or the drop-out voltage divided by the pull-in voltage. Switching voltage is the maximum voltage capable of being switched by the contacts.

PTM פורסם ב: