Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Reed Relay Overview Slide 9

To test these microscopic movements, the coil is operated at about 100 cycles per second. This will allow observation of the patterns on an oscilloscope. Operating at these speeds the mechanical dynamics are being pushed to the upper limits. The DCR is like an electrical microscope looking at the mechanical system. In this way, the DCR will show and expose any flaws in the mechanical system. These flaws represent potential early operating failures which can be eliminated and never find their way into a customer’s equipment.

PTM פורסם ב: