Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
L6470 Evaluation Kit

Using the graphical user interface, the stepping mode for the L6470 can be configured to allow the motor to run in full step or half step microstepping.  If this is set for 1/128 microstepping a nice sinusoidal current will be seen in the motor, plus a good transition through zero and a smooth current waveform.

PTM פורסם ב: