Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
dSpin Core

Another key feature of the L6470 is the dSpin core that implements a motion control algorithm in the dedicated state machine. The L6470 receives the operating parameters, like maximum speed, acceleration rate, and deceleration rate, and motion commands; such as to move a number of steps forward or reverse, go to a specific location or run at constant speed, from the microcontroller over the SPI interface. With the evaluation kit, the user can set all of these parameters from the graphical user interface.

PTM פורסם ב: