Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
open.Audio Algorithms and Hardware Slide 6

To perform the sound localization algorithm it is also mandatory to use at least two mics. That enables a selectivity of 180°. In order to achieve 360°, four mics are required. Two algorithms are available. Selecting one or the other depends on the distance of the mics. XCORR supports distance in the range of centimeters while GCC-PHAT supports in the range of millimeters.

PTM פורסם ב: