Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
VIPerPlus Slide 10

Drain current limiting with adjustable set point optimize the external component count in the system. Current limiting uses an inexpensive and lossless resistor and protects the secondary diode and the transformer from possible saturation. Fast power loop timing results in much improved transient response to rapid load changes. Finally, thanks to digital trimming at final test, the parameter distribution is the tightest in the industry. The resulting power supply features more consistent operating specifications.

PTM פורסם ב: