Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Power Inductor Basics Slide 17

The permeability of a magnetic material describes the ability of that material to contain a magnetic field inside itself (this magnetic field is generated by a current carrying conductor in the presence of the material). Permeability is one of the primary parameters used to select a core material during the magnetic component design procedure. The graph displayed here illustrates the advantage of using a ferromagnetic material over open air as an inductor core. B in the graphs here represents the Tesla, a unit used to quantify the magnetic flux density and therefore the magnetic field size. The Tesla is equal to 1 volt (V) of EMF second(s) per square meter (m^2) – (volt second per square meter)   Formula: 1T=1(V*s/m^2)    H represents the magnetizing force quantified in Ampere turns per meter. The second curve represents the permeability of a core material as the magnetizing force increases. It is apparent that after the permeability reaches its apex, the material becomes less permeable and finally reaches 0 again. At this point the core material is no longer useful to the component and it will respond to the current as an air coil.

PTM פורסם ב: