Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Power Inductor Basics Slide 9

The equation shown here represents the inductance of an air coil. By winding the conductor into a coil shape, the magnetic field generated is greatly intensified and behaves in a manner similar to that of the magnetic field of a permanent bar magnet. The permeability of free space is a known value and is used only when calculating the inductance of an air coil.

PTM פורסם ב: