Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Li98 Thermally Conductive Adhesive Tape for LED Lighting Applications Slide 14

This slide shows the typical materials properties for LI-2000. This product is available in two thicknesses depending on the roughness or concavity of the surface. The thermal conductivity is 1.2 W/mk which combined with the good adhesion strength provides an excellent way of attaching a heat sink to a substrate and also managing the thermal issues.

PTM פורסם ב: