Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Li98 Thermally Conductive Adhesive Tape for LED Lighting Applications Slide 4

Heat transfer for semiconductors is first a conduction problem, and with LED junction temperatures limited to less than approximately 100°C (in most cases), conduction is the primary transfer method until a suitable area for natural convection is reached. Radiation is small between the die and the system because the LED source is cooler than a filament or an arc. This differentiates LEDs from other lighting sources where most heat is radiated to the environment from non-LED light sources. This change in the cooling mechanism for lighting systems cannot be understated, as system designers are not used to thinking and designing for this different thermal system. A suitable path for conducting heat from the LEDs must be provided, and that also includes the various thermal interfaces in the system.

PTM פורסם ב: