Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
PCM-99 in Automotive Battery Applications Slide 14

Shown here is a chart that shows the octane performance of PCM materials, compared to PC-99, with respect to thermal impedance at a 1 mil bond line thickness (BLT). Essentially, the lower the thermal impedance the better the thermal transfer characteristics. However, this is not the only parameter to consider when selecting the material as cost and other parameters, such as re-workability or dielectric breakdown strength also need to be considered.

PTM פורסם ב: