Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
SMD-Slide4

This chart shows how increasing switching frequencies have resulted in decreasing inductor values over time. Until recently, the maximum switching frequency was 500KHz and required a 4.7µH to 10µH inductor. However, in modern devices engineers have started to use switching frequencies in the range of 1MHz to 3MHz to lower the inductance value down to 2.2µH.

PTM פורסם ב: