Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
GWS500-Slide6

Using the voltage program feature, the output voltage of the GWS500 can be adjusted over a wide range, as shown here in the slide. The bottom right hand graph shows the external voltage level required to program the output. To set the output voltage of the GWS500-24 to 28.8V for example, apply 6V to the "PV" terminal.

PTM פורסם ב: