Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Image of Telit EVB IoT Device Development Kit Quick Start Guide - Supported Mods

The Telit Cinterion evaluation board is a generic developer’s platform, which is designed to provide the complete development environment to the user and intended to be used with a set of Telit Cinterion IoT modules. The EVB is designed to carry an Interface Board (IFBD) via three 120-pin B2B connectors, thus making the EVB seamless to an actual size or pinout so that it can support multiple form factors and products. The Telit Cinterion module is mounted directly on the IFBD. The Telit Cinterion EVB supports the following modules: LE910Cx, LE910Cx - mPCIe, ME910x, and the NE310H2. In addition, all interfaces needed for the developers, such as SIM card holders, JTAG, UART, USB, audio, and microSD are available on the EVB main board.

PTM פורסם ב: