Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Circuit Isolation Techniques Slide 11

Photographs of actual construction are shown on this slide. The first is the ISO72x product, where one can see the transmit and receive chips on the left and right side respectively, connected via bond wire. The second is a cross-section view of an opto-coupler with its IR emitter on top and receiver on bottom. Finally, a picture of an inductive-based isolator where in the right image, the two transmitter coils are visible.

PTM פורסם ב: