Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Circuit Isolation Techniques Slide 7

This slide is a illustration of the benefit of isolation. The supply rails of VCC1 float with respect to those of VCC2. The offset would impact the transmission, if the receiver is unable to reject the common mode noise/frequency. Galvanic isolation makes the input, which is referenced to GND1, independent from GND2, which significantly enhances the common mode rejection.

PTM פורסם ב: