Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Dual-Mode Bluetooth Slide 5

This slide provides a high level view of classic as well as dual mode Bluetooth use cases. In the classic mode, the end node for example, tests and measures the product, and with the CC2560 device, it can connect to phones, computers or tablets where an application, which makes use of the test data and sends it over the classic Bluetooth. In the dual mode use case with CC2564 products, the end node, for example a wearable fitness monitor, can aggregate different sensor data such as heart rate from the chest strap, over BLE and then relay the aggregated data to phones, computers or tablets over classic Bluetooth for faster data transfer. This is also helpful when end devices support only classic as with some older mobile phones and PCs.

PTM פורסם ב: